Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What power distribution lugs are available for the JD, JG, JJ, and JL breaker?
Issue:
Part number for power distribution connectors for J frame breakers.

Product Line:
Molded Case Circuit Breakers

Resolution:
Below are the part numbers for the available power distribution lugs for J frame breaker:
  • PDC6JD4 - (6) #14 - #4 AWG Cu (3 lugs per kit)
  • PDC3JD20 - (2) #14 - #1 AWG Cu or (1) #12 - 2/0 AWG Cu (3 lugs per kit)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings