Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is the Powerpact D frame breaker 100% rated?

Product Line:
Molded Case Circuit Breaker

Resolution:
It is 100% rated up to 400 A. The 600 A is 80% rated.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings