Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the suffix Y followed by a 3-digit number like Y123 on the Powerpact breakers?
Issue:
Define Yxxx suffix
Product Line:
Molded Case Circuit Breakers
Resolution:
Suffix YB is special instruction or special inspection. This suffix is no longer valid on new orders for breakers. Breakers with non standard options, instruction or inspection are ordered by description and then a Yxxx ( xxx = 001 to 999) suffix is assigned.

Character Y followed by a 3-digit number (e.g. Y123) is used to define "customer special". If the catalog number exceeds 25 characters, some features/options will be combined into this Yxxx (in variable positions) so that the number of characters is 25 or less. Packing characters such as RP and Z shall remain part of the catalog number and not be placed into the Yxxx variable positions.

Examples:
PJL36080U64AE1AABCSA (20 char) + 18 in. wire harness for shunt trip = PJL36080U64AE1AABCSAY245 (24 char)

PJL36080U64AE1AABCSAJKYDYK (26 char) = PJL36080U64AE1AABCSAY271 (24 char)

PJL36080U64AE1AABCSAJKYDYK (26 char) + 18 in. wire harness for shunt trip = PJL36080U64AE1AABCSAY362 (24 char)

PJL36080U64AE1AABCSAJKYDYKRP (28 char) = PJL36080U64AE1AABCY457RP (24 char)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings