Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the number strip for NF panels?
Issue:
Number strip part numbers for NF panels

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Numbering circuits helps to identify them for connection and troubleshooting purposes.

Resolution:
NF number strips are available for circuit numbers up to 204.

NF102OE is for odd/even numbers through 102.
NF102S is for sequential numbers through 102.
NF204OE is for odd/even numbers 103 through 204.
NF204S is for sequential numbers 103 through 204.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings