Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are replacement contacts available for the Class 8810 NEMA size three two speed starters?

Yes, Class 9998 Type SL7, three pole kit, if device is 5 pole - 3 pole then two pole kit part number is Class 9998 Type SL6.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings