Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement for a M5IAI?
Issue:
Repair parts available for the Medical panel indicator M5IAI

Product Line:
Medical products sold and supported in North America

Environment:
Selection/maintenance

Cause:
Replacement

Resolution:
The M5IAI is now obsolete with no repair parts available. In order to replace the M5IAI with the current style product, the Line Isolation Monitor (LIM) will also need to be replaced. See below for the following options:
1. IG6M - LIM
2. 4800IG6CBKTVM - connector plate, harness, and mounting brackets
3. IG62000CBMST0614 - Only if the have the existing legacy box  530087BB OR
4. IG62000CBMG4 - mounts in an electrical 4 gang boxReplacement may require selection of additional components.
5. Please refer to the bulletin below for repair parts
Should you have additional questions, please contact Technical Support @ 1.888.778.2733 for further assistance.

Schneider Electric USA

Attachment(s)
4805CT1301New repair 2015.pdf [3.08 MB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings