Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an RC8L125S, Series M01?
Issue:
Repair parts

Product Line:
CSED

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056172350 (includes latch)
Load Center Cover - 7329401401
Load Center Cover Hinges - (2) X2983
Load Center Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 4056167402
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one screw is required)
Load Center Interior - 4056164050
Load Center Interior Mounting Screw - (6) 2153217161
Meter Base Assembly - 4056210850 (includes meter base with the left, load side meter jaw, blade guide, and L-shaped connector assembled to the meter base)
Meter Jaw - (3) 7329794850 (fourth is included in the meter base assembly, noted above)
Meter Jaw Mounting Bolt - (3) 2271020242 (fourth is included in the meter base assembly, noted above)
Meter Jaw Mounting Keps Nut - (3) 2342702001 (fourth is included in the meter base assembly, noted above)
Meter Jaw Blade Guide - (3) 4052761901 (fourth is included in the meter base assembly, noted above)
Line Side Phase Lugs - (2) 4025102450
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Closing Plate - (2) ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings