Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement branch switch for the old QMB210T Series 1 through 4?
Issue:
Product replacement

Product Line:
QMB branch switches

Environment:
Replacement switch

Cause:
Application and or maintenance

Resolution:
This will depend on the the existing QMB panelboard interior. The replacement switch would be a QMB323TD providing the interior is Type QM(31-inch wide) manufactured after 1961 but before October 1984 OR if the interior is type QW (38-inch wide) manufactured before 1984. If the existing interior is the QW type, with flat bus bar, the QMB310LEX plug-on extension assembly may also be required. Use the outside poles.



Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings