Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HOM612L100RB, Series 2(or 002) load center?
Issue:
Current design repair parts

Product Line:
Homeline load centers

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4055342450 (includes latch)
Cover Mounting Screw - (2) 2142717161
Interior Trim - 4055802102
Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only 2 screws are required to mount the interior trim)
Interior Assembly - 4055805750
Interior Mounting Screw - 2142217101 (2 required)
Neutral Bonding Screw - 4020502001
Closing Cap - BCAP
Notes: Replacement covers or interior trims do not have labels applied.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings