Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can single phase in, single phase out EZM branch devices be used in the same line up with 3 phase in, 3 phase out EZM branch devices?
Issue:
Can single phase IN - single phase OUT, EZM Branch devices be installed in the same line up with 3 phase IN - 3 phase OUT EZM Branch devices?

Product Line:
EZM Metering

Resolution:
No, single phase in, single phase out branch devices cannot be used in the same line up with three phase EZM branch devices.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings