Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the installer need to do to ensure an electrostatic shield is properly bonded to ground?
Issue:
Grounding Electrostatic Shields

Product Line:
LV Transformers

Environment:
Applies to Transformers by SquareD/Schneider Electric

Resolution:
SquareD/Schneider Electric`s Ventilated Transformers with electrostatic shields have the shield lead terminated at the core clamp, which is bonded to the enclosure by the factory. When the installer properly bonds the enclosure of the Transformer to the nearest earth ground, as required by the NEC, the electrostatic shield is automatically properly bonded as well.

Square D/Schneider Electric`s Sealed Resin Encapsulated Transformers with electrostatic shields have the shield lead(s), (There may be more than one), unterminated by the factory. It is the responsibility of the installer to properly bond the shield lead to ground. This is typically done when the installer bonds the enclosure to the nearest earth ground as required by the NEC.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings