Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement part number for the pneumatic timer supplied with the Class 8606 Type S autotransformer starter?
Issue:
Pneumatic timer used on autotransformer starters class 8606 type S

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8606 Type S Reduced voltage starters

Resolution:
9050AO12E, complete part number with required voltage code. Typically V02 - 120 volts..

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings