Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the QC12L200C, series M01?
Issue:
Repair parts

Product Line:
CSED

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (includes latch)
Load Center Cover - 4056157550 (includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173501
Dead Front Interior Trim Mounting Screws - 4020513001K (contains 10 screws; only 3 screws are required)
Load Center Interior - 4056161650
Load Center Interior Mounting Screws - (4) 2153217160
Meter Base Assembly - 4056189950 (includes meter base, line and load side lugs, meter jaws, meter jaw blade guides, and load side connectors)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings