Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a circuit breaker be mounted sideways so that the toggle moves left/right as opposed to up/down ?
Issue:
Mounting the breaker pertaining to handle position.

Product Line:
Miniature and Molded Case Circuit Breakers

Resolution:
Yes. NEC section 240-81 states:
"Circuit breakers shall clearly indicate whether they are in the open OFF or closed ON position. Where circuit breaker handles are operated vertically rather than rotationally or horizontally, the UP position of the handle shall be the ON position."

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings