Issue:
Are there restrictions to mounting EDB34125 branch breakers?
Product Line:
NF panelboard
Environment:
NA
Cause:
Mounting restrictions
Resolution:
If the enclosure is NEMA 3R, just one can be mounted in 400/600A panels. If the box is NEMA 1, more than one can fit in a 400A/600A panel. In Nema 1 125A or 250A interior, the panel can accept one. NO larger than a 20A EDB can be mounted across from these breakers.
Are there restrictions to mounting EDB34125 branch breakers?
Product Line:
NF panelboard
Environment:
NA
Cause:
Mounting restrictions
Resolution:
If the enclosure is NEMA 3R, just one can be mounted in 400/600A panels. If the box is NEMA 1, more than one can fit in a 400A/600A panel. In Nema 1 125A or 250A interior, the panel can accept one. NO larger than a 20A EDB can be mounted across from these breakers.
Released for: Schneider Electric USA