Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where can the breaker adapter kit part EZM125QOA be installed in the EZM metering?
Issue:
Product Features

Product Line:
EZM metering

Resolution:
EZM125QOA adapter kits are used to convert a bolt-on 2p tenant circuit breaker position to a plug on style tenant circuit breaker position in the following meter center branch units:

MPL units that make use of bolt on, 2p, 70 - 225 A, QBP-TM, QDP-TM, QGP-TM, or QJP-TM tenant circuit breakers can use this adapter with 2p, 40 - 125 A, QO, QO-VH, or QOH circuit breakers.

EZM, EZMR, EZMH, or EZML branch units that make use of 2p, 100 - 200 A, Q2M, Q2M-VH, or Q2MH circuit breakers can use this adapter with 2p, 40 - 100 A, QO, QO-VH, or QOH circuit breakers.

EZM, EZMR, EZMH, EZML, or EZMT branch units that make use of 2p, 100 - 225 A, QDP-TM, QBP-TM, QGP-TM, or QJP-TM circuit breakers can use this adapter with 2p, 40 - 125 A, QO, QO-VH, or QOH circuit breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings