Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the largest ampere rating of the EZM main breaker devices?
Issue:
Current product design

Product Line:
EZM Metering

Resolution:
The largest ampere rating of the EZM main breaker devices is 2000 A. The catalog numbers of the EZM, 2000 A main breaker devices are as follows: EZM12000CB, EZM12000CBU (does not meet EUSERC),  EZM32000CB, or EZM32000CBU (does not meet EUSERC).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings