Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are tandem QO, 30 A breakers available?
Issue:
Is there a QOT breaker rated at 30A?

Product Line:
MIniature Circuit Breakers

Resolution:
There is no QOT3030, but a QO3030 is available (non CTL type). This is not listed for use in CTL style panels, though. If the panel is marked CTL, there is no option for a 30 A, tandem QO breaker.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings