Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do we make an equipment ground fault breaker for the NF panel?
Issue:
Is there an equipment ground fault breaker available for the NF panel

Product Line:
Panelboards

Environment:
NF Panelboards

Cause:
Application

Resolution:
Yes.  EDB, EGB, EJB breakers are available with 30 mA ground fault protection.  These circuit breakers have the suffix of EPD (Equipment Protective Device).  They  are available in one pole 277 volt rated 15 to 50 amps.  Each of these circuit breakers occupy 2 pole spaces.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings