Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the heavy duty safety switches available with factory installed copper lugs?
Issue:
Product selection

Product Line:
Heavy Duty Safety Switch

Resolution:
No, all the copper lug kits for heavy duty safety switches are ONLY available for field installation. The copper lug kits are not available on NEMA 7/9 or 800 - 1200 A switches.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings