Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can any of the EZM branch units that are configured for 3-Phase IN and 1-Phase OUT be field converted to 3-Phase IN and 3-Phase OUT branch units?
Issue:
Product Design features

Product Line:
EZM metering equipment

Resolution:
No, field conversion of branch devices that are 3-Phase IN - 1-Phase OUT CANNOT be converted to 3-Phase IN - 3-Phase OUT. This would void the UL listing and violate the NEC.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings