Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are single phase K13 transformers available?
Issue:
Single phase K13 rated Transformers.

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Resolution:
K rated Transformers are usually Three Phase because the presence of harmonic energy overheating the Transformer is typically a problem seen with Three Phase systems.  Single Phase systems rarely have a need for k rated Transformers.  There are on occasion quotations for Single Phase k13 Transformers, but they are increasingly rare.  However. These are available and must be quoted on a special basis through the local field office.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings