Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What configurations, receptacles and QO breakers are provided in ALL the Servicepak, Power Outlet Panels(or PAK devices)?
Issue:
Product Design Features

Product Line:
Servicepak Power Outlet Panels

Environment:
Recptacles and configurations

Cause:
Applications

Resolution:
NOTE: This FAQ is ONLY for showing the configurations, the receptacles and QO circuit breakers used in each Servicepak, Power Outlet Panel catalog number. This FAQ is NOT for determining ANY other product information. For all other product information, see the current on-line digest or each catalog number CAD drawing.

1) The configuration for each catalog number is shown in the below tables 1.95 and 1.96, under the column heading - "Power Outlet Configuration". That configuration will match what is shown to the left of the table 1.95 under the heading "Configurations".
2) The receptacle types for each catalog number are shown in the same tables, under the heading "Receptacles(Included)", with the quantity of each receptacle type under a letter. That letter corresponds with the receptacle types shown in the lower left corner to the tables under - "Receptacle Types".
3) The QO circuit breakers contained in each catalog number, that feed each receptacle are shown under the table heading "Circuit Breaker(Included)".

For Example: The catalog number PAK10C1 has the configuration 1C and contains one type 'A' receptacle which is a 20A, 125V, 2W and Grnd-NEMA 5-20R and is fed from a QO120GFI breaker installed.



PAK Device Digest table

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings