undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the maximum ampere rating available for the EZM main devices, both single and three phase?
Issue:
Product Design Features

Product Line:
EZM Metering

Resolution:
The maximum ampere rated EZM main circuit breaker device is 2000 A.

The maximum ampere rated EZM main fusible switch device is 1200 A.

The maximum ampere rated EZM main terminal box device is 2000 A.

Schneider Electric USA

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: