Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the location of the 5th jaw on the EZM, EZMH, EZMK, EZML, or EZMR branch device and what 5th jaw is used?
Issue:
Application

Product Line:
Multi Metering

Resolution:
NOTE:
ALL sockets include 5th jaws factory installed except the EZMK and EZM11____ devices, which are all 4 jaw meter sockets
It will depend on the device catalog number.
1) EZM prefix units that are supplied with 5th jaws have the 5th jaw factory installed in the 9 o'clock position. When needed, the 5th jaw can be moved in the field to either the 3 or 6 o'clock position, depending upon local utility requirements.
2) EZMH, EZML and EZMR prefix units(1-phase out) are all supplied with 5th jaws installed in the 9 o'clock position. When needed, the 5th jaw can be moved in the field to either the 3 or 6 o'clock position, depending upon local utility requirements.
3) EZML and EZMR prefix units(3-phase out) are supplied with the 5th jaws installed in the 6 o'clock position. When needed, the 5th jaw can be moved in the field to either the 3 or 9 o'clock position, depending upon local utility requirements.
NOTE: If a 5th jaw is required, the part number is 5J

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings