Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are there alternate lugs for the 600A HCP14506 interior, that will accept (3) - 4/0 conductors per phase?
Issue:
What alternate lugs is there available for the 600A HCP14506 I Line panel board interior?

Product Line:
I-Line panelboard

Environment:
Terminations

Resolution:
There are no alternate lugs for this wire size and amount, per phase. For this lug size and conductor amounts, using the 800A, HCP14508 I Line interior, will allow for landing (3) 3/0-500 kcmil wire per phase.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings