Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the lug range for the PBCF5A100TB?
Issue:
Lug range for the PBCF5A100TB?

Product Line:
Busway

Environment:
Product Features

Resolution:
The phase lugs in the PBCF5A100TB will accept wire from #6 to 300kcmil. The ground lug will accept copper wire from 2/0 to #10 and aluminum wire from 2/0 to #6.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings