Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will a QO-GFI work on a two pronged receptacle that has no ground conductor?
Issue:
Will a QO120GFI work on a receptacle that has no ground?

Product Line:
QO/HOMELINE Circuit Breakers

Resolution:
Yes, it will work without a receptacle ground conductor. The system does need to be solidly grounded, though.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings