Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do 200 amp 35 kV loadbreak one piece bushings and loadbreak inserts have the same loadbreak elbow interface?
Issue:
Loadbreak elbow interface on 200amp 35kV transformer.

Product Line:
Transformers

Environment:
North America Products

Cause:
N/A

Resolution:
No. One piece bushings use an ANSI/IEEE Std. 386 Fig 8 interface. Inserts use an ANSI/IEEE Std. 386 Fig 7 interface. The elbows are not interchangeable.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings