Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can EZM main lugs tap boxes (400 A - 2000 A) be installed as service equipment?
Issue:
Product Design Feature

Product Line:
EZ METER-PAK Multi-Metering Equipment

Resolution:
Yes, the following EZM tap boxes are suitable for use on the LINE side or LOAD side of service equipment.
They are shipped with isolated neutrals and each is supplied with a neutral bonding kit for use when required.
EZM1400TB, EZM1400TBU, EZM1600TB, EZM1800TB, EZM1800TBCU, EZM1800TBU, EZM11200TBU, EZM11600TB, EZM12000TB;
EZM3400TB, EZM3400TBU, EZM3600TB, EZM3800TB, EZM3800TBCU, EZM3800TBU, EZM31200TBU, EZM31600TB. EZM32000TB.

Note, that the 225 A tap boxes (cat. no.: EZM1225TB and EZM3225TB) are supplied with isolated neutrals that cannot be bonded, and cannot be used on the LINE side of service equipment.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings