Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the NF 400 amp panel with a LC main breaker and 54 circuits be changed from main breaker to main lugs?
Issue:
Change fom MB to ML an NF 400A panel with a LC main breaker and 54 circuits

Product Line:
Panelboards.

Environment:
Products sold in North America

Cause:
Product features

Resolution:
No it cannot be changed as it is built completely different than the other 400 amp NF main breaker panels.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings