Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a main circuit breaker for single phase load centers that is rated higher than 22 kAIC?
Issue:
Do we have a main breaker for single phase load centers that is rated for higher than 22 kAIC?

Product line:
Residential load centers

Resolution:
No. The QOM1 and QOM2 type main breakers for single phase load centers are both rated at 22 kAIC, the highest available AIC rating for a single phase load center.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings