Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included in the SO1020VP and SO2040VP Combination Service Entrance Device Value Packs?
Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Components included in Value Pack

Issue:
Application

Resloution:
The SO1020VP includes
(1) SO1020M100S CSED, Ring type, 4-jaw meter socket, Overhead feed ONLY, Surface mount, with a 100amp Main breaker feeding a 10space-20circuit load center
(3) HOM120 (Homeline 20amp single pole branch circuit breaker)
(3) HOMT2020 (Homeline, 20amp Tandem single pole branch circuit breaker).


The SO2040VP includes;
(1) SO2040M200S CSED, Ring type, 4-jaw meter socket, Overhead feed ONLY, surface mount, with a 200amp Main Breaker feeding a 20space-40circuit load center.
(4) HOM120 (Homeline 20amp single pole branch circuit breaker)
(1) HOMT2020 (Homeline 20amp Tandem single pole branch circuit breaker)
(1) HOM230 (Homeline 30amp, two pole branch circuit breaker)
(1) HOM250 (Homeline 50amp, two pole branch circuit breaker)

Schneider Electric USA

Explore more
Product:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings