Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does HVL switchgear come with padlock provisions for locking in the open and closed positions? Are there padlocking provisions on the fuse door and optional rear door?
Issue:
Padlocking provided on the HVL switchgear

Product Line:
HVL switchgear

Environment:
Products sold and used in North America

Resolution:
Yes, all doors have a padlock hasp which protrudes through a slot in the door. The handle is locked open or closed with the slotted holes in the crank casting.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings