Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the EZM Main Devices(main breaker, main fusible switch or main terminal box) be used for overhead(top) and/or underground(bottom) feed?
Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Installation

Cause:
Application

Resolution:
It will depend on the catalog number for the EZM main device.
NOTES: a) ALWAYS CHECK WITH THE LOCAL UTILITY FOR APPROVAL BEFORE USING.
b) ALWAYS CHECK THE INDIVIDUAL CAD DRAWING FOR EACH DEVICE CATALOG NUMBER BEFORE USING.

1) The EZM main catalog numbers with suffixes of 'CB', 'FS', 'TB', 'CBC', 'CBCMS' would be UL listed for both combination overhead(top) and underground(bottom) feed.
2) The EZM main catalog numbers with suffixes 'CBU', 'CBE', 'CBUMS', 'CBEMS', 'FSB', 'FSU', 'FSE' and 'TBU' would be UL listed for underground(bottom) feed ONLY.
3) The EZM main catalog numbers with suffixes 'CBT', 'FST', 'CBTMS', would be UL listed for overhead(top) feed ONLY.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings