Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you mount an SL800 subfeed lug kit on the right or left hand side of the bus stack in an HCW panelboard?
Issue:
Mount an SL800 subfeed lug kit on one of the sides of the bus stack in an HCW panelboard

Product Line:
I-LINE Panelboards

Environment:
Products sold and used in North America

Cause:
Installation / Setup

Resolution:
An SL800 subfeed lug kit can not be installed on either side of an HCW I-Line panelboard. The HCW has a branch ampacity limit of 600A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings