Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is it possible to obtain a bucket for a Model 6 Motor Control Center similar to a catalog number 8998SBF070 with two 70A circuit breakers?
Issue:
Get a bucket for a Model 6 Motor Control Center similar to a Cat number 8998SBF070 with two 70A circuit breakers

Product Line:
Motor Control Centers

Environment:
Products sold in the North America

Cause:
Availability

Resolution:
Square D/Schneider Electric no longer builds dual circuit breaker feeder buckets for Motor Control Centers. However, it is possible to use two Compact units, catalog number 8998HBF070 in this application. In this case two 6`` units will fit in the same space as one 12`` unit.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings