Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does XUX0ARCTT16 come with the Reflector for use in the ``Polarized Retroreflective`` mode or the Transmitter for use in the ``Thru-Beam`` mode?
No, the reflector or the transmitter must be ordered separately. There are several models of relectors available. The XUZC50 is the most commonly ordered.The Transmitter catalog numbers are as follows:
XUX0AKSAT16T is 12-240vDC and has a 2 meter (6.6 foot) cable
XUX0AKSAM12T is 12-240vDC and has a 4 pin micro connector
XUX0ARCTT16T is 24-240vDC and has a 2 meter (6.6 foot) cable


CTA-ID : 2028316

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings