Issue:
Product design features
Product Line:
EZ Metering
Resolution
No. a 1 phase device cannot be added to a 3 phase EZM line up. It would require a 3 phase tap box (example: EZM3800TB) to be used when the meter center has a 3 phase horizontal cross bus.
BEFORE obtaining the terminal box, verify with the local utility and code authority for approval of application.
Product design features
Product Line:
EZ Metering
Resolution
No. a 1 phase device cannot be added to a 3 phase EZM line up. It would require a 3 phase tap box (example: EZM3800TB) to be used when the meter center has a 3 phase horizontal cross bus.
BEFORE obtaining the terminal box, verify with the local utility and code authority for approval of application.
Released for: Schneider Electric USA