Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between standard Masterpact NW and NT breakers and Masterpacts with LF and L1 ratings?
Inquiry:
What is the difference between standard Masterpact NW and NT breakers and Masterpacts with LF and L1 ratings?  Do they have different trip units?

Product Line:
Masterpact NW

Resolution:
Masterpact L1F and LF NW breakers use the same trip units as the standard breakers. The difference is in the design of the arc chamber. The current path has a reverse current loop which passes current in one direction through the stationary terminal and moveable contact arm in opposite directions. This creates a strong repulsive force resulting in quick contact opening before the breaker trips and it also magnetically forces the arc into the arc plates to segment and cool the arc with the effect of reducing arc energy. They do NOT use fuses.

Schneider Electric USA

Attachment(s)
Masterpact Low Arc-Flash Curves.pdf [44.19 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings