Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type and size of hub is used on the individual and horizontal ganged meter sockets?
Issue:
Product Design Features

Product Line:

Individual Meter Sockets and Horizontal Gang Meter Sockets

Resolution:
Both the A type (1" up to 2.5" sizes) and the A-L type (2.0" up to 4.0" sizes) can be used on the individual and horizontal gang metering devices.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings