Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will an FC frame breaker fit into an HCM panel?
Issue:
FC frame breaker fit into an HCM panel.

Product Line:
Panelboard

Environment:
HCM panel

Cause:
N/A

Resolution:
Yes, however, the panel label will not list the FC as an acceptable breaker. Note , an HJA breaker is a comparable option to the older FC .

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings