Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of mains are provided on a HOM816U200FTRB load center?
Issue:
What are the mains that is provided on a HOM816U200FTRB load center?

Product Line:
Load Center Circuit Breaker

Environment:
Homeline Circuit breaker

Resolution:
This device is a ``Universal Mains`` load center, which is not initially supplied with a main device. A Main Breaker Kit or a Main Lugs Kit can be field installed as the application may require. To use as a Main Lugs load center, order and field install a QOL225. To use as a Main Breaker load center, order and field install a QOM2-VH Main Breaker Kit, 200A maximum. Catalog numbers for available Main Breaker Kits would be QOM2100VH (100A), QOM2125VH (125A), QOM2150VH (150A), QOM2175VH (175A) or QOM2200VH (200A).

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings