Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What Combination Service Entrance Devices come standard with a factory installed Main Breaker(Service Disconnect)?
Issue:
Product Design feature

Product Line:
Combination Service Entrance Devices (CSED)

Environment:
Service Disconnect or Main Breaker

Cause:
Application

Resolution:
CSED = Combination Service Entrance Device
MB(SD) = Main Breaker(Service Disconnect)


**** ALWAYS PAY ATTENTION TO ANY FOOTNOTES ASSOCIATE WITH EACH CATALOG NUMBER, ON THE DIGEST PAGE, BEFORE OBTAINING ANY DEVICE****

To determine what CSED come standard from the factory with a MB(SD) installed and what type of MB(SD), SEE THE CURRENT ON-LINE CSED DISGEST PAGES OR EACH CATALOG NUMBER CAD DRAWING. SEE BELOW LINKS
NOTES:
1) The column headings of the digest tables will point out the CSED that contain a factory installed MB(SD) and the column information will show what type is used. SEE THE BELOW VISUAL.
2) At the beginning of the CSED digest pages is a Catalog Logic that will also show if the MB(SD) is factory or field installed.

Current On-Line Digest = Current On-Line Digest
On-Line CAD Drawing system = CAD Drawing

BELOW ARE A COUPLE VISUAL EXAMPLES OF THE CSED DIGEST PAGES SHOWING MB(SD) TYPE, MAX. AMPERAGE AND IF FACTORY INSTALLED OR NOT.
img1
img2

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings