Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the horn bypass kit part number MMHB be used for both the MP Meter-Pak meter centers and the EZM branch devices?
Issue:
Product Accessories

Product Line
MP Meter Pak and EZM Metering

Resolution:
Yes, but only with the below stated devices:
The horn bypass kit MMHB kit can be field installed on the Ringless Type Meter-Pak catalog number prefixes 'MPR'.
The Ringless type Meter-Pak catalog number prefixes 'MPH', come standard with Horn bypass factory installed and the horn bypass kit MMHB can be used for field replacement.
The horn bypass kit MMHB CANNOT be used on the Ring Type Meter-Pak catalog number prefixes 'MP'.

For the EZM Metering branch devices:
The horn bypass kit MMHB can be field installed on the Single Phase ONLY EZM Meter Branch device catalog number prefixes 'EZMR'(5-jaw).
The EZM catalog number prefixes 'EZMH' come standard with Horn Bypass factory installed and the horn bypass kit MMHB can be used for field replacement.
The horn bypass kit MMHB CANNOT be used on the Ring Type EZM branch device catalog number prefixes 'EZM'.
The horn bypass kit MMHB CANNOT be used on the EZM branch device catalog number prefixes EZML, EZMK, or 3phase EZMR(7-jaw) devices.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings