Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the recommended fuses for use with control transformer kit, 9999 CPT1D1, when applied with a 240V primary?
Issue:
Recomended fuses for control transformer kit.

Product Line:
Transformer

Environment:
North America Product

Cause:
N/A

Resolution:
With a 240V primary, 1A fuses are recommended, with a maximum rating of 1.04A permitted using the 250% rule of NEC450.3. Please note the fuses are to be 600V maximum, 1-1/2 x 13/32`` Class CC rejection type, time delay fuses (Bussmann Type FNQ-R or equivalent). Qty (2) are required. On the 120V secondary side, a 1.25A fuse is recommended, with a maximum rating of 1.39A permitted according to the 167% rule of NEC 450.3. Provisions are for qty (1) fuse, which must be 1-1/2 x 13/32``, non-rejection type fuse (Bussmann type FNQ or equivalent).

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings