Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the EE version of the obsolete catalog number 15S1H?
Issue:
Cross reference

Product Line:
Low voltage dry type transformers

Environment:
NEMA

Cause:
Changes to the required operating efficiencies for low voltage ventilated dry type transformers have resulted in the obsolescence of some catalog numbers.

Resolution:
The EE version of the 15S1H is catalog number: EE15S3H.  Please note that there are significant dimensional and weight differences in these transformers.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings