Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for a 300A/3p Circuit Breaker Unit for an old QMB Saflex Panelboard?
Issue:
300A/3P circuit breaker replacement for the old QMB Saflex panelboards/switchboards.

Product Line:
Obsolete QMB panelboards and switchboards

Environment:
Replacement

Cause:
N/A

Resolution:
Use a QMB3300LA . A QMB310EX Plug On Extension Assembly is also needed if the panel is a QW type , the box is 38``w and the bus is flatwise . Note this CANNOT BE INSTALLED IN QM STYLE PANELBOARDS PRIOR TO 1961.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings