Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a 'B'- phase connector supplied with QMB, 2 pole switches so the installer can phase balance the loads in the QMB panelboard or switchboard?
Issue:
Product Design Features

Product Line:
QMB Safety Switches

Resolution:
Yes. The switch is built with AC phase connections. The B phase connector is supplied with the switch so the installer can convert to AB or BC phase connections as required to balance the loads.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings