Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data of the EZM32000CB, series M01 main breaker device?
Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Resolution:
The RJF36200 circuit breaker is used as the main breaker in this device. The EZM device is rated for (6) 1/0 - 750 kcmil Al/Cu or (12) 1/0 - 250 kcmil Al/CU wires per phase and neutral. The ground lug will accept (1) #6 - 300 kcmil Al/Cu wire.

NOTE: The ONLY alternate lugs are compression lugs, BUT they will not allow for more wires or a larger wire size.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings